6/30/2012 12:21 PM | |
Joined: 4/14/2010 Last visit: 2/8/2025 Posts: 525 Rating:
|
Greeting, Could you please help on following issue in Netpro Config. (see attached) Warning: Please make sure that all ports of the CP in PROFINET IO mode to which PROFINET IO devices are connected can be operated at 100 Mbps full duplex. Avoid the use of hubs. Thanks, AttachmentNew folder.zip (75 Downloads) |
MS |
|
Follow us on