1/21/2014 1:21 PM | |
Posts: 1368 Rating:
|
Hello Brian, do you upgrade the non-working SCALANCE X308 to FW 3.7? If yes, does the SCALANCE X308 had Bootloader 3.27.5 before? Then you must note the following point: Please use this Firmware 3.7.0 only with Bootloader Version higher than V3.27.5! If the Bootloader Version is lower than or equal to V3.27.5, please update to the Firmware Version V3.7.2! Otherwise, please update your non-working SCALANCE X308 to FW 3.7.2 http://support.automation.siemens.com/WW/view/de/61615844 Hope, it solves your problem... |
1/22/2014 1:10 PM | |
Posts: 16 Rating:
|
I did not change the firmware on any of the switches, I am not sure if one of my co-workers have done so in the past, maybe, maybe not. The switches have all been bought at different times over the last years, so they have many different firmware versions! I upgraded the switch to firmware 3.7.2 and now learning works it seems! I will do so if I encounter another switch with the same problem, thank you! |
This contribution was helpful to
1 thankful Users |
Follow us on