5/20/2021 7:12 AM | |
Posts: 16 Rating: (0) |
AARRGGHH I get sooo frustrated. Everything is working just like you described :-) but now i have run in to a new problem. Scaling analog input. i looked in the forum on other posts and only found one with the "same issue" in that post they showed a picture of the problem but i didnt see the solution or explanation. i have a specific range on my sensor. like 0 to +100 or -30 to + 70 -30 to +70 works in the min max and gain and offset, but try to use 0 - 100 it goes red all over and want me to use 1 to 105 or 104 i cant remember now. ok so 0 to 1000 works i just need to divede it by 10 i think. in with a math instruction but no :-) is there any good videos / documents that actualy explain how to do this ?because the help dont give any hints :-( should i use 2 amplifiers in series ? ------------------------------------------------------------------------------------------ |
Last edited by: ThomasGC at: 05/20/2021 07:13:42Last edited by: ThomasGC at: 05/20/2021 07:16:54Last edited by: Jen_Moderator at: 05/21/2021 07:31:51New subject after splitting |
|
5/20/2021 7:49 AM | |
Joined: 12/18/2014 Last visit: 4/30/2024 Posts: 32908 Rating: (4069)
|
I think I know what you mean. |
5/20/2021 8:26 PM | |
Joined: 12/18/2014 Last visit: 4/30/2024 Posts: 32908 Rating: (4069)
|
Soory, in my screenshot in the post above is a fault . The gain of the second amplifier must be 0.1, not 1.0. |
5/20/2021 8:33 PM | |
Posts: 16 Rating: (0) |
yes to divide the first value by 10 ;-) figured that much it is working on the Logo i just need to adapt the ranges on the HMI now and test it out :-) |
5/20/2021 8:49 PM | |
Posts: 16 Rating: (0) |
deleted |
Last edited by: ThomasGC at: 05/20/2021 21:09:40 |
|
5/20/2021 8:49 PM | |
Joined: 12/18/2014 Last visit: 4/30/2024 Posts: 32908 Rating: (4069)
|
Please don't show a screenshot, but upload the program as a zipped file. |
5/20/2021 9:01 PM | |
Joined: 12/18/2014 Last visit: 4/30/2024 Posts: 32908 Rating: (4069)
|
In B006 you don't divide the value from analog amplifier trough 10, you add 10. |
5/20/2021 9:17 PM | |
Posts: 16 Rating: (0) |
i dont get it ! :-( i thought i am taking the result from the B002 and this i have to divide with 10 to get the right value. when it is 1000 it have to be 100 that is /10?? but yes it is not working when using /10 then the value is 32767 but when i use + 10 the 0 % value is 10 and the 100% value is 1010 Attachmenttemp 2.zip (173 Downloads) |
5/20/2021 9:27 PM | |
Joined: 12/18/2014 Last visit: 4/30/2024 Posts: 32908 Rating: (4069)
|
And with the correct settings you became the right results ... Attachmenttemp 2_V2.zip (159 Downloads) |
5/20/2021 9:31 PM | |
Posts: 16 Rating: (0) |
Please kick me :-) Rookie mistake. Like you said i was adding 10 i didnt get the "system" the + - / * under the value is of course for the line below not the line above :-( simple math it is working now here is the file Attachmenttemp 2.zip (172 Downloads) |
5/20/2021 9:32 PM | |
Posts: 16 Rating: (0) |
ahh you posted the file the same time i posted my answer :-) Thank you so much for your help Have a nice evening |
5/20/2021 9:45 PM | |
Posts: 16 Rating: (0) |
Properly a broken foot ;-) https://photos.app.goo.gl/6Mbz13sZG8AsbYbg7 |
Last edited by: ThomasGC at: 05/20/2021 21:47:15 |
|