6/20/2022 3:56 PM | |
Joined: 7/8/2019 Last visit: 6/16/2023 Posts: 12 Rating: (0) |
Thank you very much mr. V ! Following this manual; v20_operating_instructions_complete_en-US_en-US.pdf i see the the following; P0777 x1 -9999 <> 9999 % output scaling (but think 0% is same as 0HZ) P0778 y1 analog output scaling 0-20 (so 0 or 4(mA) will do the job) P0779 x2 of analog output scaling -9999<>9999% (default 100% so i need to calculate *) P0780 y2 of analog output scaling 0-20 (keep it on default 20mA) The calculation i assume to be made; 20mA / 8.8mA = 2.27 so the percentage of increasing the output value will be 227% ? Thanks again |
Last edited by: Jen_Moderator at: 06/21/2022 08:21:04Link optimized. |
|