7/6/2012 9:09 PM | |
Joined: 9/24/2009 Last visit: 4/21/2024 Posts: 2 Rating: (0) |
Helo, Gabriel. In your attachment OSCAT_V11.zip missing file OSCAT_V11.al11 and I can't open library.
|
7/9/2012 10:30 PM | |
Joined: 2/16/2011 Last visit: 4/4/2024 Posts: 229 Rating: (27) |
Dear App$, Problem solved.
|
Gabriel de Oliveira |
|
10/2/2012 7:30 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349)
|
Today Siemens released an SCL Conversion tool (Deutsch/English language only) for free download. It batch converted the entire OSCAT SCL library uploaded in this thread. I zipped up the entire folder (attached). Some things will not work no matter what you do because of the significant differences between S7-300/400 & S7-1200. However, this conversion seems to fix lots of the problems encountered during the conversion, some of which I had not run across with this library of open source logic. It is a big package that unfortunately cannot simply be compiled into a single library and then be used as is - there are duplicate scl source files in multiple directory locations, but each folder can be a self-contained library. AttachmentOSCAT_After_SCL_Converter_ForTIAPortal_V1x.zip (1615 Downloads) |
science guy |
|
This contribution was helpful to7 thankful Users |
Follow us on