6/16/2021 11:34 AM | |
Joined: 2/16/2021 Last visit: 9/7/2022 Posts: 5 Rating:
|
Thanks for this. I get it to work with your project file and also if I ad a new panel and screen to my project. However, screens on my "old" panel in the project (transferred from v16) only shows 6 items under "Controls" and "System.diagnostics control" is not one of them. Are there some configuration I have to change somewhere to allow this? "System diagnostics" is checked under "Controller alarms" in "Runtime settings". Edit: I got it to work after updating the firmware version to 17.0.0.0. ------------------------------------------------------------------------------------------ |
Last edited by: Einads at: 06/16/2021 15:59:27Last edited by: Jen_Moderator at: 06/21/2021 09:56:24New subject after splitting. Inserted quote. |
|
This contribution was helpful to
3 thankful Users |
Follow us on