5/7/2020 11:24 AM | |
Joined: 5/20/2019 Last visit: 5/14/2025 Posts: 14 Rating:
|
Hello, after searching a lot on simens forum and in google, i haven't found useful for taking screenshot and saving as image on windows ce panel. I have also tried captce and few others software but didn't work anything. Therefore, I have created my own windows ce application for capturing screen during runtime. Which, I would like to share with you. please find attachemnt HMIScreenshot.zip I have keep it very simple. All photos will be saved in the folder "HMIScreenshot" in same directory, where software is located. Now you can place this software in your USB/SD card and call it through "Startprogram" in runtime. If you want to take photos of all screen then you can use "Activatescreen" in VBS to call all screen one by one and call HMIScreenshot.exe . For example: ActivateScreen "ScreenName", 0 StartProgram """\Storage card USB\HMIScreenshot.exe""", "", hmiShowNormal, hmiNo Note: If HMIScreenshot.exe doesent work then you need to update compact framwork 2.0 or above. You can update compact framwork using SIMATIC Prosave software. Compact Framework V2.0 is also attached. ★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ ★★★If this post did really help you, you may use the Rate-button ★★★ ★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ AttachmentHMIScreenshotandCFV2.0.zip (1165 Downloads) |
This contribution was helpful to
11 thankful Users |
8/19/2021 1:38 PM | |
Joined: 7/26/2016 Last visit: 10/1/2024 Posts: 1 Rating:
|
Thank you! |
5/24/2022 8:25 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by Da Prada Davide is split to a separate thread with the subject Is it possible to remove date and time from the file name?. Best regards |
Follow us on