2/5/2025 6:34 PM | |
Joined: 1/21/2025 Last visit: 3/5/2025 Posts: 5 Rating:
|
Sim0mN, I have another problem. My PC / screnn are in 1920*1080 My project are in 1366*768, the ratio is the same for PC and project resolution, it's fine. My projects are all in 1366*768 dur to keep compatibility to 19" screen an 10" screnn. But I have a problem for the placement of Pop-Up In the screen If my screen is in 1366*768 all is correct. I calculate the position of my Pop-Up dynanimaticaly. Case 1: Left position of the Pop-Up is align to another object position. Case 2: Left position of the Pop-Up is calcuated to be in the center of the screen - Left Position = (Screen client resolution - Popup Width) / 2 When my PC/Screen is 1920*1080 and runtime is autosized the position of the Pop-Up is not correct. I have'nt find the solution to know by script teh resolution of the the pc to apply a ratio. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/06/2025 08:29:21New subject after splitting |
|
2/5/2025 6:42 PM | |
Joined: 10/6/2018 Last visit: 4/10/2025 Posts: 60 Rating:
|
Hello Please have a Look at this Forum entry I‘ve pretty much done what you need here if i understand it right Hope it works for you too |
Best Greetings / Schöne Grüße |
|
Follow us on