Industry Online Support
Technical Forum
8/11/2022 10:21 AM | |
Joined: 10/22/2020 Last visit: 4/17/2024 Posts: 169 Rating: (6) |
Hi mlhoffmann, could you please specify which settings you would like to modify? For example, is it the configuration of the I/O interfaces or the network connections? In general, everything can be achieved from your request. You can customise files in the operating system from a Python script, which can be used to configure the network interfaces, for example, up to the point that you can execute complete Linux shell commands. When it comes to updating via git, I recommend a .yaml file. You can first have this pulled in a script and then refer to it in your Python script. For automated execution at every system start, you can use a bash script or write the "git pull ..." and Python programme call directly in the bashrc of your operating system. The most elegant solution is to generate a system service for the python script like here. Feel free to give us feedback on how your application looks exactly. Wishing you success. BR |
Follow us on