11/8/2024 9:53 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello AutoGen_1839426 first of all you should delete the temp files of the Project and do test also in Simulation: https://support.industry.siemens.com/cs/de/en/view/109778709 Do you see some differences? In Comfort Panels the script queue is working one by one. SO f you run a Script that takes very long or blocks (in case of an endless loop) other scripts will not be executed in time. You can try to visualize some performance indicators with Option+: https://support.industry.siemens.com/cs/de/en/view/109754400 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on