1/3/2024 7:23 AM | |
Joined: 8/17/2022 Last visit: 4/15/2025 Posts: 15 Rating:
|
Hello SIr, I am currently experiencing the same problem. I use scripring to change my screens. It is working flawless in the simulation, but screens are skipped or not shown correctly when using the HMI in realtime.... Pressing longer on the button sometimes helps. It is as if two command cannot be handled at the same time when pressing a button.... In my case, when pressing the "OK" button, the footer should change and the screenwindow_body also.... This sometimes works fine, sometimes NOT.... Maybe it is better to only change the Screenwindow Body, and then perform an 'Onloaded' action and change the footer when the Screenwindow Body is loaded... I suspect a poor scanning of both commands when pressing a button or incorrect event handling... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/03/2024 10:08:12New subject after splitting |
|
Follow us on