6/30/2016 1:28 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (194) |
Hello javed88, with WinCC Comfort you can't do that with a control. Here are some links that might help you:
Aside from these... Maybe you can use the script in the FAQ linked below. It tells you if the memory card can be written on. If it's full you obviously can't.
If you have only one archive it only uses a kinda fixed amount of memory. Maybe it's better to put the full archives on a network drive?
|
Last edited by: H.J. at: 6/30/2016 1:37:31 PMLast edited by: H.J. at: 6/30/2016 1:39:15 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on