6/28/2013 2:53 PM | |
Posts: 123 Rating:
|
Hello, What is the maximum SD memory card size supported by the multi (WINDOWS CE 5.0) and comfort panels (WINDOWS CE 6.0)? (max. 2GB?) How should the SD card be formatted? e.g.: - SIMATIC HMI TP1900 COMFORT - SIMATIC MP 377 How about usb memory? |
6/28/2013 3:11 PM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello Bofely, Perhaps this link might help: Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
6/28/2013 4:19 PM | |
Posts: 123 Rating:
|
Thanks. But it doesn't give an anwser to my questions. |
6/29/2013 9:45 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hi bofely, Entry ID: 21847868 SIMATIC HMI Memory Card MMC - Siemens ... As far as I know officially for TP 1900 panels is 2GB and for MP 377 is 512 MB. |
Last edited by: Ste39 at: 6/29/2013 10:17 AMLast edited by: Ste39 at: 6/29/2013 10:15 AMLast edited by: Ste39 at: 6/29/2013 10:13 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on