Industry Online Support
Technical Forum
7/24/2014 10:10 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! Please checkthis topicfirst. Then you can try to look atSIPLUS modulesfor extended temparature ranges. For the technical data gohere. For example, of extended range: SIPLUS S7-300 SM321 - 20-POLE -40 ... +70 DGR C WITH CONFORMAL COATING CONFORMITY WITH EN50155 T1 KAT 1 KL A/B BASED ON 6ES7321-1BH02-0AA0 . DIGITAL INPUT OPTIC. ISOLATED 16 DI, 24V DC, 1 X 20-POLE Hope it helps |
7/24/2014 10:43 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello S_F, Example for "Standard CPU" 0..60 °C Go to Ambient condition: Product data sheet 6ES7315-2EH14-0AB0 - Industry Mall - Siemens |
Last edited by: Ste39 at: 7/24/2014 10:45 AM |
|
7/24/2014 10:53 AM | |
Posts: 16 Rating: (0) |
Hi Ste39, That's what made me tensed, now planning to go for Siplus, Thanks, |
This contribution was helpful to1 thankful Users |
Follow us on