Industry Online Support
Technical Forum
11/23/2009 3:42 PM | |
Posts: 131 Rating: (0) |
Dear all, could u help me find the equivalent (attached) flowmeter in Siemens ultrasonic flowmeters? it's a flume channel and i need 250 and 600 m3/h flow rate respectively. all remaining details are the same as the one attached. i appreciate ur help.tnks.
Attachmentflowmeter.zip (196 Downloads) |
11/23/2009 4:35 PM | |
Joined: 3/29/2007 Last visit: 1/31/2022 Posts: 14 Rating: (2) |
Hi Patrik, Open channel measurement, our product most accuracy, is the OMC III. Attached the catalogue page. You need select the transducerfor complete the selections. Regards Santiago Thomassey AttachmentOCM III.zip (197 Downloads) |
10/28/2010 4:08 AM | |
Posts: 64 Rating: (2) |
In order to accurately measure flow with a parshall flume, flow velocity must also be measured. The is no velocity sensor available for the OCMIII. |
Follow us on