8/7/2016 5:24 PM | |
Joined: 4/28/2015 Last visit: 5/27/2022 Posts: 29 Rating: (0) |
Dear All,
|
8/8/2016 12:28 PM | |
Posts: 84 Rating: (8) |
Hello, If you need a real time trend that will be simple by using adress multiplexing but for data log trend as I know you need to create a trend view for each tag because it's not allowed to dynamize the process value in the trend view properties. There is a project example for long-term archiving, it could help you. How do you do long-term archiving with WinCC flexible? |
Last edited by: Z.BolBol at: 8/8/2016 5:16:22 PM |
|
8/8/2016 8:35 PM | |
Joined: 4/28/2015 Last visit: 5/27/2022 Posts: 29 Rating: (0) |
Hi Z.BolBol Unfortunatelly i need to use archive. Next time i will simply buy Wincc Professional. Regarding the project example that you suggest me to see i have one important question. This is exactly what i should do as a second step. Is there any way to load diffrent archives with this method or there is the same problem that i faced for the trends so i will have to do 300 pages for long therm archive? The solution described here https://support.industry.siemens.com/cs/document/60520367/how-can-you-graphically-display-the-contents-of-the-tag-archive-of-a-comfort-panel-or-the-wincc-runtime-advanced-on-the-pc-without-wincc-(tia-portal)-?dti=0&lc=en-WW is not accepted because it's too complicated for the client. I should do everything in runtime. |
Last edited by: Floowkid at: 8/8/2016 8:36:56 PM |
|
8/10/2016 10:11 AM | |
Posts: 84 Rating: (8) |
Hello Floowkid, I tried this this method with about 30 trends and it works well for me.
Create a text list with 300 values (1 for "Trend n°, 2 for "Trend n°2",...) and then dynamize your trend views visibilities with the selected trend number.
When the user change the trend number you execute a script which copy the selected tag archive to the Trend archive and to do so take a look in the load_archive script in the attached project example. How do you do long-term archiving with WinCC flexible?
|
8/25/2016 3:17 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
Hello Floowkid, you can use the example project of the following application example as training material. It is the TIA Portal Version of the project linked by Z.BolBol.
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
8/25/2016 5:29 PM | |
Posts: 84 Rating: (8) |
Hi Floowkid, Here is a project example with 5 trends, you can just adapt it to display 300 trends. Regards AttachmentPC_Runtime_Selection_Archive_Trend_View.zip (679 Downloads) |
This contribution was helpful to1 thankful Users |