9/27/2010 3:54 PM | |
Joined: 9/27/2006 Last visit: 3/21/2025 Posts: 12344 Rating:
|
Hello mankar; Here are a few documents on the CP 341, and a sample program (in pdf) that you can use to set your own test project. CP 341 ASCII sample program: http://support.automation.siemens.com/WW/view/en/6894849 Manuals:CP 341 Point-to-Point Communication, Installation and Parameter Assignment Manuals, configurable:CP 341 - First Steps in Commissioning If you are new with the CP 341 or PtP comms, I recommend you spend some time reading the manuals, until you understand the sequence required to set up the CPs: hardware available and inter-CP wiring, parameter selection and settings, function blocks to be programmed. This will save you much trouble when you start looking at the sample program and writing your own. Hope this helps, Daniel Chartier |
Follow us on