11/11/2015 11:40 AM | |
Posts: 9 Rating:
|
Hallo, I am using Serial communication for the first time. I am trying to send string to a Printer using RS232 Hardware through FB3 S_Send. When I trigger S_Send, there is no change in DONE or ERROR (both are FALSE) . I am evaluating them with an OR to SET a Temp variable. I don't see any chance. STATUS is #0. S_RCV shows ERROR as TRUE and DONE as FALSE and STATUS #1E0E. It would be great, if someone could help. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/11/2015 2:44:11 PMNew subject after splitting |
|
11/11/2015 6:19 PM | |
Posts: 3093 Rating:
|
Hello Swaroop, Regards, |
11/12/2015 3:42 PM | |
Posts: 9 Rating:
|
Thanks a lot. This solved the problem. |
This contribution was helpful to
1 thankful Users |
Follow us on