3/18/2011 3:35 AM | |
Joined: 10/7/2005 Last visit: 4/17/2025 Posts: 3047 Rating:
|
Hello safety4ever you can definetely NOT use AG_SEND/AG_RECV (FC5/6, max 240 Bytesfor ISO connections in a 400). You can however use either: AG_LSEND/AG_LRECV (FC50/60, max 8192 Bytes lenght for ISO connections in a 400) OR AG_SSEND/AG_SRECV (FC53/63, max 1425 Bytes lenght for ISO connections in a 400) and attached is a pic from thehelp on these Blocks which contains all these limits. Whatever you do you, please make sure to have a look atTHIS link (which has plenty of examples and further links) and also to pay heed to the connection establishment and TSAP"rules" contained in entry ID 17661306 which are:
TSAP rules
I hope this helps |
Last edited by: fritz at: 3/18/2011 3:37 AMuploaded pic Cheers |
|
Follow us on