2/6/2012 3:38 PM | |
Posts: 2 Rating: (0) |
I´m sry, maybe it is stupid question but, where can I find there TM_MAIL command? Not in TIA portal, so where? Thanks |
Last edited by: majkl at: 2/6/2012 3:42 PM |
|
2/6/2012 7:59 PM | |
Joined: 12/12/2008 Last visit: 4/18/2024 Posts: 69 Rating: (6) |
Yes it`s in the TIA portal. You must have theTIA SP2. You will find the block under "Communication->Teleservice" |
This contribution was helpful to1 thankful Users |
2/9/2012 10:12 AM | |
Posts: 2 Rating: (0) |
Works perfect. Thanks |
3/1/2012 4:25 PM | |
Posts: 7 Rating: (3) |
Get rid of the TCON command, you don't need it. I don't have it in my code and it is not required. |
3/1/2012 11:54 PM | |
Joined: 3/11/2007 Last visit: 4/14/2024 Posts: 226 Rating: (13) |
Here is available for download an example of sending email. Hello /tf/WW/en/Posts/67185#top |
This contribution was helpful to2 thankful Users |
10/31/2012 9:52 AM | |
Joined: 3/2/2012 Last visit: 5/6/2024 Posts: 1 Rating: (0) |
Does someone have a working example? i've bin trying to get the TM_MAIL working, i do not see what i'm doing wrong. |
10/31/2012 2:51 PM | |
Joined: 7/7/2010 Last visit: 5/6/2024 Posts: 14680 Rating: (2350)
|
Look up just a couple of posts to the one by automatizzando. Follow their link to just near the end and find their posted example. |
science guy |
|
1/31/2013 2:40 PM | |
Joined: 10/22/2008 Last visit: 5/6/2024 Posts: 365 Rating: (5) |
What I would like to add to the post is that I tried TM_MAIL few days ago and works ok. - smtp server with 25 port open - 1214 -1hg31- FW 3.0.2 - TM_MAIL v 1.1 - TIA v11 SP2 UP5 P.S. The eWONdevices looks very nice. Is it really so easy to use? Is it the sameas VIPA devices? |
1/31/2013 5:55 PM | |
Posts: 7 Rating: (3) |
As a Siemens distributor here in the U.S., I probably can't discuss Ewon devices in their forums. All I can say is, YES, they are VERY easy to use, and I have many customers using them to access their Siemens-based systems all around the world. I have no idea if they make them for VIPA or not. Frankly, I was hoping Siemens would simply "buy" Ewon and market them as Siemens products because they work so well with Siemens products via ethernet OR Profibus. ;) I also wish Siemens would some day allow us to modify the Port 25 address. I know somebody stated in this thread that it can be modified, but I don't believe that to be true at all. Good luck! |
Follow us on