9/4/2018 10:45 PM | |
Posts: 439 Rating:
|
At this point, if your computer is connect to internet, you are able to test the above configuration with the simulator. |
9/4/2018 10:52 PM | |
Posts: 439 Rating:
|
Select "PN_X1" and make sure you have the correct IP address, subnet mask and gateway. Here are the DNS server I usually use. |
9/4/2018 10:58 PM | |
Posts: 439 Rating:
|
Download into the HMI, click on "Start" button of the "Start center", click on the button and that's it! |
This contribution was helpful to
1 thankful Users |
7/11/2022 1:10 PM | |
Joined: 2/27/2018 Last visit: 2/8/2023 Posts: 1 Rating:
|
Hi, I do have de same problem, any idea? |
Follow us on