4/25/2013 12:39 PM | |
Posts: 1547 Rating:
|
Hello, there's an application available here: http://support.automation.siemens.com/WW/view/en/25545680 Which explains the basic settings as well as a library the sends / receives SMS. |
2/6/2014 1:24 PM | |
Posts: 123 Rating:
|
i am interresting about your feedback, i am actually building a similar application using also 314, and CPrs232, but in my case i have TC35i regards
|
2/6/2014 1:32 PM | |
Posts: 1368 Rating:
|
Hello S44, in your post /tf/WW/en/Posts/102847 i noticed, that there is a difference between these module while the initialization. The code for MD720-3 implements the command AT+CPMS= "MT". This does not exists with the TC35. Here, it is AT+CPMS = "SM". The same with AT+CNMI=2,0,0,0,0 (MD720) and AT+CNMI=(0/1/3),0,0,0,0 (TC35) Perhaps you can proof these commandos via Hyperterminal and AT+CNMI=? and AT+CPMS=? and look the answer of the modem TC35. Have you done it yet? |
Follow us on