10/3/2019 10:54 AM | |
Joined: 5/25/2018 Last visit: 7/11/2022 Posts: 10 Rating:
|
Dear Experts, I have a project using Wago 857-400 and I have a question. Please help me in this case. 6ES7214-1AG40-0XB0 – PLC S7-1200 CPU 1214C DC/DC/DC 6ES7231-4HF32-0XB0 – Module S7-1200, ANALOG INPUT, SM 1231, 8 AI Wago 857-400 (support 2 cable) Conductivity sensor (4 wrire with 4 meter cable support). Now I want to connect sensor to analog module (far away 20 meter) Is it ok if I use the Wago 857-400 to link sensor & analog module using 4-20mA ? How to connect 4 wire sensor to Wago 857-400 (Isolator)? Thank for your support. AttachmentWAGO 857-400.pdf (101 Downloads) |
10/5/2019 7:04 AM | |
Joined: 5/25/2018 Last visit: 7/11/2022 Posts: 10 Rating:
|
Dear My Friend, Thank you for your information. It helps me a lot. {snip} ------------------------------------------------------------------ For follow up question see: connect to PLC via RS485: I don't have static IP, my solution is use Teamview VPN. |
Last edited by: The Helping Hand at: 10/07/2019 10:23:35Split follow up question to new thread. |
|
This contribution was helpful to
1 thankful Users |
Follow us on