12/14/2016 8:18 AM | |
Joined: 4/23/2010 Last visit: 3/23/2023 Posts: 8025 Rating:
|
Yes you may connect provided links to be disconnected between 1U1, 2U1 1V1 2V1 & 1W1 2W1. But with this connection & if there is phase angle difference or phase reversal & if some one connects the links, heavy short circuit may damage the module. Moreover when original connection is retained, 2U1, 2V1 & 2W1 supply is provided thru commutating reeactor which is more safe.
No, it is not designed for single phase & moreover how & where you will connect neutral?
No. Please read the detail manual here.
|
This contribution was helpful to
1 thankful Users |
Follow us on