10/31/2011 1:41 PM | |
Posts: 3037 Rating: (192)
|
Hello, The download does not work with any adapter. You should see the following FAQ for MPI download. How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Tweety |
11/2/2011 8:15 PM | |
Posts: 54 Rating: (0) |
Yes, the resistors are correct, I am using the PC adapter from the CPU to the PC. Yesterday a made transfers but the remote control is not working. |
11/3/2011 4:54 PM | |
Posts: 3037 Rating: (192)
|
Hello, You do a download for your project from computer to a panel. PC/MPI-Adapter is not released for download to a panel. You can see this in this FAQ: What transfer options are available in the various operator panels? See the document "Projecttransfer_V1_2_e.pdf Tweety |
11/7/2011 11:28 AM | |
Posts: 3037 Rating: (192)
|
Hello, You can download your Step 7 project about a PC/MPI adapter. You can download your WinCC flexible project about MPI to OP77B or TP177B. You can not download your WinCC flexible project about a PC/MPI adapter. The MPI download about PC/MPI adapteris not tested and not approved for panels OP77B and TP177B. You must use the MPI download without this PC/MPI adapter. See in the manual, page 54. SIMATIC HMI WinCC flexible 2008 Communication Part 1 You can see this notice on the page 54. Notice The PC adapter is not approved for MPI transfer. |
11/9/2011 11:16 AM | |
Posts: 3037 Rating: (192)
|
Hello, You can use the MPI transfer about a CP, for example CP 5512 or CP 5611. You can use another kind of transfer (serial). How can you transfer a WinCC flexible project serially to a panel? You need for serial transfer to OP77B a RS 232 cable. What is the serial cable assignment for transferring the configuration to a Windows-based device? You need for serial transfer to TP177B a RS 232 Multimastercable. What transfer options are available in the various operator panels? |
11/11/2011 9:38 AM | |
Posts: 3037 Rating: (192)
|
Hello, You should use PROFIBUS cable with PROFIBUS connectors with resistor for your MPI communication. PROFIBUS connectors You should integrate your WinCC flexible project in Step7. How do you integrate a WinCC flexible project in STEP 7? Then you can interconnect the panels and CPU in STEP 7 ( NetPro). Tweety |
Last edited by: Tweety at: 11/11/2011 9:38 AM |
|
11/14/2011 10:16 AM | |
Posts: 3037 Rating: (192)
|
Hello, Do you have enough OP Communication Connections in HW Config? You find fhissettings, Properties of your CPU > folder "Communication". Tweety |
11/24/2011 4:27 PM | |
Posts: 3037 Rating: (192)
|
Have you set the first and the last resistor of the connector?
Have you set "the Panelis only master on the bus" on the panel, PC/PG interface settings and your WinCC flexible project? The parameters of the transfer settings in the Control Panel are overwritten from the parameters of the WinCC flexible project.
The following FAQ can you see for connection between Panel and PLC via Profibus. How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? Tweety |
Follow us on