3/29/2016 8:52 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Hello, Is the path of the target OS set correctly? It looks like you download your ES instead of the OS. |
If I could help you, you can use the RATE button. Thank you. |
|
3/29/2016 9:49 AM | |
Posts: 567 Rating: (106) |
hi, check also the Points of the following FAQ: |
3/31/2016 7:05 PM | |
Joined: 8/19/2012 Last visit: 5/22/2024 Posts: 125 Rating: (0) |
thank to all best regard
Attachmenterroe1.docx (63 Downloads) |
4/23/2016 4:13 PM | |
Joined: 8/19/2012 Last visit: 5/22/2024 Posts: 125 Rating: (0) |
hi all i found simatic shell some errors as attachement .so i chose the correct network but still no being from ES to both server . can i download without used the being or necessary being between ES and both servers. best regard Attachmentsimatic shell.docx (67 Downloads) |
7/13/2016 6:33 PM | |
Joined: 9/3/2008 Last visit: 5/24/2024 Posts: 922 Rating: (158) |
Hi, I suggest that you make a lmhost file (remember the file has no extension. The name is "lmhosts").
|
Last edited by: Michael K at: 7/13/2016 6:34:26 PMMichael |
|
Follow us on