6/21/2010 5:43 PM | |
Joined: 9/27/2006 Last visit: 3/26/2023 Posts: 11997 Rating:
|
Hello Solution Riders; You are asking questions that go deep inside the PCS 7 configuration, and that could require a lot of research. For starters, you could look at the following FAQ, very detailed: http://support.automation.siemens.com/WW/view/en/19353091How do you create a SIMATIC PCS 7 V6.0 SP3 project with S7-400 station, pair of redundant servers and client? You will alsofind there a link to the Applications section of Siemens Support that will give you pointers on how these configurations can be used for a PCS 7 v. 7 configuration. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/21/2010 8:12 PM |
|
This contribution was helpful to
1 thankful Users |
6/21/2010 7:51 PM | |
Joined: 11/15/2009 Last visit: 3/13/2023 Posts: 375 Rating:
|
Hi Solution riders The manul is too helpful.SIMATIC Process Control System PCS 7 Compendium Part A - Configuration Guidelines Regards |
6/23/2010 6:21 AM | |
Joined: 4/19/2008 Last visit: 1/17/2023 Posts: 1525 Rating:
|
Hi Solution Riders, Here is the link for the Minimal Configuration PCS 7 V7.1,Which will help you for the Configuration. |
Ammy |
|
6/24/2010 2:44 PM | |
Posts: 112 Rating:
|
dear friends, Can i have the pdf document for assigning of server data package....?. |
Follow us on