10/12/2020 3:55 PM | |
Joined: 10/11/2006 Last visit: 2/6/2023 Posts: 5416 Rating:
|
Hello, there is no command for continue available. You have to do it applicative. There is an application "Laxisctrl" who supports this. SIMATIC S7-1500 / S7-1500T: Standard application axis control https://support.industry.siemens.com/cs/ww/en/view/109749348 2.2.2 Functions of basic motion coordinate system There are different modes for jog functionality available: Mode 0: Continuous jogging – axis is moved at velocity / speed setpoint as long as a jog input is set. Mode 1: Incremental jogging – every rising edge at a jog input starts a new increment Mode 2: Incremental jogging – continue the last increment until it is completed. After finishing a new rising edge starts a new increment.
|
With best regards, |
|
Follow us on