5/14/2008 3:59 PM | |
Posts: 5822 Rating: (412)
|
Hello, well this list is fully sufficient, I would say. With this list you can hardcode your Connection points in your Program, no question. If you would get a Symbolic list you can be a bit more flexible, especially if something changes in the PLC but anyway. The Symbolic list can be imported in the Symbolic Editor in SIMATIC NET and theConfiguration Console within SIMATIC NET. Good luck J_Bell |
5/20/2008 10:26 AM | |
Posts: 14 Rating: (0) |
First of all thank you for prompt answer. I have further work on it and now i'm in this situations: who is working with the program will not use the symbolic name. So I have the list with the DB where I can exchange the data. Now my problem is: How can I define the OPC point in the server since I dont have the program and without use a PLC ? I mean, if I define in Simatic Net the configuration, then when Im connecting with the OPC scout I can see only a red cross on the DB and I can not add any point with address DBXXX. I would like to have the DB that I need, so I can define the point in the OPC server and finally get the point in my HMI with the OPC client defined on it. Thank you for the answer, Lebowski. |
5/20/2008 5:59 PM | |
Posts: 5822 Rating: (412)
|
Dear Lebowski, there we have the Problem. J_Bell |
Follow us on