7/28/2014 9:33 AM | |
Joined: 11/26/2009 Last visit: 3/7/2024 Posts: 213 Rating: (1) |
hi, Please look at the CPU properties , perticularly you can look at the clock memory.
|
7/28/2014 9:57 AM | |
Joined: 4/24/2006 Last visit: 5/17/2024 Posts: 8649 Rating: (1151) |
Hello, Could it be, there is used OB100. (Start up OB) Best regards, Wizard |
8/2/2014 10:43 PM | |
Joined: 7/20/2009 Last visit: 1/16/2024 Posts: 61 Rating: (3) |
pratik7332what to check? Wizardi have an OB100 but i dont use the M10.0 anywhere in the project vipzi only use a reset of M10.0 and the contact of the M10.0. I dont have any other set of M10.0. Any other idea?
|
8/7/2014 7:44 PM | |
Joined: 7/20/2009 Last visit: 1/16/2024 Posts: 61 Rating: (3) |
I attach a photo of the connection of I1.0 and M10.0 I dont have the I1.0 or the M10.0 anyware else in the program.
|
8/7/2014 9:37 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, Did you or did you not check your System and clock memory bytes? This is why we asked multiple times. How can you avoid overwriting the flags that are allocated for system and clock memory bits in the user program? M-bits do not set themself, so it must be set by program, hardware settings like clock/systemmemory or HMI. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |