2/7/2013 11:24 AM | |
Posts: 2 Rating:
|
Helloo I've been trying to set (Ethernet) communication between 2 s7-300 CPUs with bsend and brcv blocks using PLCSIM. The problem is I'm still getting an error with status "1" I created the project on step7 v11(please check the attached file) the project works quite well when i donwload on the plcs but when using plcsim i don't have a data transfer i am also having the error status 1 on both bsend and brcv please help me with this AttachmentTESTNET.zip (65 Downloads) |
Last edited by: O_Moderator at: 2/11/2013 11:47 AMnew subject after splitting from /tf/WW/en/Posts/82281#top |
|
2/11/2013 11:52 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread PLCSIM_S7 300_ STEP 7 V11 Best regards O_Moderator |
Follow us on