Industry Online Support
Technical Forum
4/23/2010 2:52 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating:
|
Hi Manuelzes, the script engine of Windows CE differs from the on of a PC. So, any access to the shell is impossible, for instance. But I don't get the idea behind your script. It makes no sense to set the system time always to the same value. There you can find a FAQ, how to handle the time on Panels: http://support.automation.siemens.com/WW/view/en/24104104 Or use a simple Date-Time field with the mode "Input/output" to set the time of the panel. If it must be handled by script, you have to use the area pointer "Date/Time PLC" with additional tags. In this case, the FAQ above isalso good for understanding the handshake beetween panel and PLC. |
mfG / Best regards |
|
Follow us on