4/21/2008 5:56 AM | |
Posts: 487 Rating: (36) |
Hi I am not a WinCC specialist but have a look at these links , it may help you in understanding your problem ... Link1 and Link2 Eric |
4/21/2008 11:08 PM | |
Posts: 6 Rating: (0) |
Aykona, yes it's the same popup https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=15252277&nodeid0=10805583&load=content&csQuery0=start+server+locally&subtype=130000&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW Siemens has wrote: " Note: Ok, but why avant my problem I have a different situation? I dearchive the project on same machine....Where is set in the operating system or Simatic, the information of my configuration system? Wednsday I will try to download the project on the server machine (I configure a virtual machine with the same configuration).. then i will write here the result.. Thank's Sergio |
Follow us on