10/12/2023 3:54 PM | |
Joined: 10/4/2022 Last visit: 10/18/2023 Posts: 3 Rating:
|
Hello to all, in the enclosed project everytime i press F1 the counter value cyclically goes from 1 to 4. I would like to set M1 if the counter is 1, M2 is the counter is 2, M3 if the counter is 3 and M4 if the counter is 4. Can anyone help me? Regards Luca Attachmenttest.zip (30 Downloads) |
10/12/2023 4:35 PM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
You can use analog threshold triggers by using Parameter VM Mapping.. Take a look at Tools > Parameter VM Mapping Attachmenttest_V2.zip (31 Downloads) |
This contribution was helpful to
1 thankful Users |
10/12/2023 5:58 PM | |
Joined: 6/11/2019 Last visit: 12/5/2023 Posts: 1961 Rating:
|
Hello Inoxgan1, or via a muxer with differential threshold switches. Ella_68 (translated with Google) Attachmenttest_V3.zip (34 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on