8/13/2014 2:26 PM | |
Joined: 5/17/2010 Last visit: 12/7/2024 Posts: 226 Rating:
|
Hi OwainW, SIRIUS Softstarters do not have reversing contactor inside. There is just a Slow speed function which can be used in both directions for positioning or maintenance work for example by special thyristor control (see chapter 6.4). If you want to realise a reversing starter application with softstarter then you can use the circuit diagram which is included to 3RW44 manual at chapter 9.1.9 or 9.1.10 Manual SIRIUS 3RW44 Soft Starters http://support.automation.siemens.com/WW/view/en/21772518 Kind Regards Michael . |
Last edited by: Mr. SIRIUS at: 8/13/2014 2:26 PM------------------------------------------------------------------------------------------------ |
|
8/13/2014 2:38 PM | |
Posts: 2 Rating:
|
Lovely, Thank you very much for your help |
Follow us on