7/26/2014 10:43 PM | |
Posts: 5225 Rating:
|
Hi there, Some of the older panels needed to be placed into download mode. ..if I remember correctly you could place it in "serial" download mode or "MPI" download mode. - - the point is.. it will be most helpful if we knew what HMI you are using with your "S7 319 PLC". Do however look into the suggestion that Ste39 made and let us know if this resolved your issue. Greetings. w |
7/28/2014 6:27 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello Isbell, Please have a look: You can use this: How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? and take a look if your CPU supports Routing: Which modules support the S7 routing function? |
Follow us on