3/16/2015 7:14 AM | |
Posts: 1299 Rating:
|
Hello, if you start the simulation (with the start simulation button in TIA portal) of the comfort panel, the sm@rtserver is also simulated. To access the sm@rtserver you need to set a password in control panel > WinCC Runtime Advanced Internet tab "remote" > change settings. K!ke |
3/16/2015 12:23 PM | |
Posts: 1299 Rating:
|
Hello, if it's possible, I would recommend you to update to SP1, because the problem is solved with this version. If it's not possible, here is an article with the alternatives: https://support.industry.siemens.com/cs/ww/en/view/101977510 K!ke |
3/18/2015 7:52 AM | |
Posts: 1299 Rating:
|
Hello, is the panel connected to the internet? you have to configure your panel for remote access. https://support.industry.siemens.com/cs/ww/en/view/26662448
K!ke |
Follow us on