10/6/2008 10:33 AM | |
Joined: 4/6/2006 Last visit: 1/21/2019 Posts: 604 Rating:
|
Hi, Yes normally you can. I advice here to use a W78x Access Point together with the IWLAN/PB Link PN IO you have mentioned. It's possible to connect up to 8 PB Devices behind the IWLAN/PN Link PN IO. I think it's an indoor application I will recommend you to use 5 GHz which is allowed in Denmark. Keep in mind that the signalstrength is sufficient and that both antennas have a clear line of sight with a lot of room. If the antennas are in a small area it could be that there are so many reflections from it self that's disturbing the signal too much for PN IO traffic. It really depending on the PN IO update times you need or this could work wihtout the problems. Advice for an antenna would be the ANT795-6DN which can work in both 2,4 and 5 GHz. Recommended for this kind off aplications are normally RCoax solutions which is for material not much more expensive then what you use know. Maybe installating the equipment will be harder with RCoax. RCoax Manual |
Best regards, |
|
Follow us on