12/24/2014 7:34 AM | |
Posts: 1064 Rating: (72) |
can you post your diagnostic buffer are you losing communication to the fm355 card , possible change the bus connector |
12/24/2014 11:11 AM | |
Joined: 2/1/2011 Last visit: 9/13/2023 Posts: 186 Rating: (4) |
Sir, Please find the hardware configuration and diagnose of PLC. kindly provide me the solution as soon as possible. Thanks
AttachmentDetails.zip (572 Downloads) |
1/8/2015 10:43 AM | |
Joined: 2/1/2011 Last visit: 9/13/2023 Posts: 186 Rating: (4) |
Sir, Please find the details of Diagnostic buffer of PLC. This fault comes suddenly and as we make plc stop and restart again then it stars working okay. FM card changed, PLC changed but still problem could not be rresolved. It comes randomly and in a week two or three times. Kindly suggest me the working to do for resolving this problem.
AttachmentDiagnose_C_D.zip (486 Downloads) |
Last edited by: ashishm at: 1/8/2015 10:44 AM |
|
1/12/2015 9:38 AM | |
Joined: 2/1/2011 Last visit: 9/13/2023 Posts: 186 Rating: (4) |
Dear All, Still waiting for reply.
|
1/20/2015 5:50 AM | |
Posts: 56 Rating: (2) |
CHECK THE FORUMSIMATIC S7-300 / S7-300FOB 122 |
7/25/2019 6:42 AM | |
Posts: 2 Rating: (0) |
...sent from App |
7/25/2019 6:44 AM | |
Posts: 2 Rating: (0) |
S7 fault problem show in s7 300 cpu in some time time interval and reset . Some time automatucally reset or some time need power resatrt . |
7/25/2019 7:34 AM | |
Joined: 9/21/2012 Last visit: 9/9/2024 Posts: 4127 Rating: (463) |
And what are the messages in Diagnostics buffer of the CPU? |
Follow us on