2/24/2011 6:17 AM | |
Joined: 10/7/2005 Last visit: 6/1/2023 Posts: 2966 Rating:
|
Hello ryan3 You are using a 31xC CPU aren't you? (SFB48 is only for these types of CPU's). If so,the links below should give you the answers: How do you use the built-in function "Frequency Measurement " of the S7 CPU 31xC? CPU 31xC Technological Functions I hope this helps |
Cheers |
|
2/25/2011 6:09 AM | |
Joined: 11/9/2009 Last visit: 4/4/2023 Posts: 41 Rating:
|
sr my qustion is in wher input i will put the sensor signal to the sfb 48,thanks sr |
2/25/2011 6:30 AM | |
Posts: 1064 Rating:
|
Where your input goes depends on your hardware and hardware configuration , This is explained in the manuals that Fritz mentioned |
12/14/2019 10:36 PM | |
Joined: 2/4/2011 Last visit: 5/25/2023 Posts: 4 Rating:
|
Normally the input is I124.0 (standard). |
Follow us on