2/21/2014 10:39 AM | |
Joined: 2/21/2014 Last visit: 9/23/2022 Posts: 13 Rating:
|
Where can I find information describing the returns from SFB52 for S120/S110. |
2/21/2014 2:05 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
... see: http://support.automation.siemens.com/WW/view/de/29157692 |
7/1/2021 4:27 PM | |
Joined: 3/7/2019 Last visit: 12/12/2022 Posts: 1 Rating:
|
Those only speak about G120. |
7/2/2021 5:43 AM | |
Joined: 4/23/2010 Last visit: 1/29/2023 Posts: 7962 Rating:
|
Hello, It also depends on type of telegram selected, controller etc. etc., so it is difficult to provide your desired information. You may refer below links or serach here in forum to understand application of SFB 52 & 53 block. SINAMICS S: Speed Control of a S120 with SIMATIC S7-300 ...Sinamics S120 -CPU314 PN: SFB52 - Entries - Forum ...Function blocks to control the SINAMICS with ... - AWC, Inc. |
Last edited by: Jen_Moderator at: 07/02/2021 09:11:30Optimized link. |
|
Follow us on