10/1/2012 3:43 PM | |
Joined: 1/15/2009 Last visit: 4/19/2024 Posts: 316 Rating: (40)
|
wisnia33, Ok Thank you for that information about the CFC 8.0 SP1, I have re-tested and have reproduced your same exact error. What is also not very good is that you cannot run the SIMATIC Manager New Project Wizard. Although it does state per the compatibility matrix that this is supportedhttp://support.automation.siemens.com/US/view/en/2334224, at the moment I would revert back to CFC 8.0 upd1 until something is fixed with the current version, or wait for the release of PCS7 V8.0 SP1 (not sure when that is). But it appears the issue is larger than just SFC editor.
|
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
10/2/2012 8:38 AM | |
Joined: 12/10/2010 Last visit: 3/25/2024 Posts: 2 Rating: (0) |
Hi Wisnia, I have the same problem and same error, PCS7 V8.0 udate 1, CFC V8.0 + SP1 |
1/29/2013 11:26 AM | |
Posts: 836 Rating: (99)
|
Hi, I had a simmilar problem these days and wanted to give the solution. This problem is solved with CFC V8.0 SP2 which can be downloaded here: http://support.automation.siemens.com/WW/view/en/62883989 |