4/6/2021 8:24 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello Sandeep Bakoliya, you can not migrate the SFC18 (Alarm_S) in TIA Portal for the S7-1500. I recommend to check whether it is possible to use the "Program_Alarm" in this case. See also the example (link) and the chapter with "Program_Alarm" in TIA Portal: Configuration of Messages and Alarms in WinCC (TIA Portal) With best regards |
This contribution was helpful to
1 thankful Users |
Follow us on