2/2/2022 10:29 AM | |
Joined: 12/4/2020 Last visit: 2/17/2022 Posts: 3 Rating:
|
Is there anyway to share internet LAN P1 to P2 ? Thanks, Nuttavat Boonrod |
2/3/2022 10:05 AM | |
Joined: 4/28/2015 Last visit: 8/4/2022 Posts: 2894 Rating:
|
Hi, yes that is possible! I found this very good post / instructions and tested with the IOT2050 and Example Image V1.2.1. My setup was: Router -- X2 IOT2050 X1 -- X1 IOT2040 IP Settings on IOT2050:
IP settings on IOT2040:
Additional config in the IOT2050:
Additional confing in the IOT2040:
You can use the same settings for the IOT2050, but of course you need to check what is required for the devices using the shared internet connections. Best regards! |
Out of office until Thursday, August 11th |
|
Follow us on