Industry Online Support
Technical Forum
11/16/2007 6:09 PM | |
Posts: 14 Rating:
|
Hi Mex, You might want totrigger a script on the change of a variable. Toggle a boolean or increase a INT in your CPU every 5 seconds and add anOnChange event to that tag (See Tag property /Events /Change value) I think it's also possible to get an event from the user logon handler but i don't have Flex around at the moment to verify that. Or you can get the actual log on level from the PLC and change visibilty of the button according that value. I might have an example, if required you can email me at tiesto@s7tools.com. good luck, Tiesto |
11/29/2007 8:13 AM | |
Posts: 54 Rating:
|
You can use scheduler to execute a script which will determine current user by GetUserName (as I remember) system function |
Follow us on