6/7/2020 7:39 AM | |
Joined: 8/18/2016 Last visit: 10/18/2023 Posts: 4 Rating:
|
Hello All, I want to show all the my PLCs LED status and Diagnostic buffer on HMI. Below is configuraion, 1) I have 8 PLCs each is IM 151-8 PN/DP CPUs in one project, programmed in Simatic manager V5.6. 2) HMI is TP1900 comfort configured by TIA V15. I know that if both the PLCs and HMI programmed in same TIA environment it is possible to show. But as in my project configuration software for both the PLCs and HMI are different i dont know how to show PLCs LED status and Diagnostic buffer on HMI. If i have only one PLC in my project than might be its possible with PLC proxy added in HMI, but here i have 8 PLCs in project. Can somebody help me to solve this mystery. Thanks in advance. Regards, Mitul ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/08/2020 06:52:00New subject after splitting |
|
6/12/2020 10:12 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello you can use the Object "System diagnostic view" Here are some information: https://support.industry.siemens.com/cs/ww/en/view/61910954 Or you use a html Browser Control and view the integrated websites of the PLC in the Panel Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on