2/8/2018 10:39 PM | |
Posts: 4 Rating: (1) |
Dear SICAM PAS connaisseurs, In one of our current projects, we have to integrate an ABB RET670 ver 2.2.1 relay in a SICAM PAS V8.08 with IEC61850 Ed2 communication. After engineering the protection functions and all required signals (in DataSets and RCBs) in PCM600, I export the ICD file for a collegue to import to SICAM PAS. Our receipe for third party device integration in the PAS consists of the following steps: 1) export device ICD file; 2) edit ICD file and replace manually "TEMPLATE" by the correct IEDname; 3) change modified ICD file extention to CID; 4) import CID file to SICAM PAS. The CID file import to SICAM PAS performs ok (no errors). However, in UI Operation we get the following error message: “9: Type information unavailable. Check device configuration for IEC61850, check ICD/SCD for device.” When I connect to the relay with IECBrowser and I start reporting on an RCB, I can see the reports coming with every signal state change. In attachement, the ICD file of the relay. Any idea on how to solve this issue is more than welcome. Many thanks, Regards, Alex B AttachmentRET670_ICDfile.zip (167 Downloads) |
2/9/2018 7:31 PM | |
Posts: 4 Rating: (1) |
Yes, we already tried, but the result is the same. However, I launched a wireshark capture when starting the relay communication in UI Operation. Please find attached the capture file. SICAM PAS : 172.16.1.1 RET670: 172.16.21.1 It seems that the PAS requests for a certain object that does not exist in ABB relay's configuration ("LLN0$DC$NamPlt" in LogicalDevice "MON"). The "NamPlt" DO exists only in "LD0" and "SYS" LDs. Attached, also wireshark and PCM600 printscreens. Any idea why does the PAS ask for this not-existent object? Should it be there but it isn't? Cheers, Alex Attachmentwireshark_and_printscreens.zip (146 Downloads) |
Follow us on