6/10/2022 6:09 AM | |
Joined: 4/6/2021 Last visit: 2/13/2025 Posts: 22 Rating:
|
Dear Sir I need to comission sinamics Siemens drive G 120 (6SL3224-0BE37-5UA0) I am completely new in this drive 1.Need to run the motor with potentiometer input in run command and reverse with reverse command. 2.fix speed input digital input for jog forward and reverse if required. 3.E-Stop and off command 4.addtion of braking resistor 5.motor rating is 75kw, 3 phase, 415 a input, Rated current 138A, rated speed 750, rated frequency 26 hz and required toreque is 97.5 kgfm 6.need to configure one MPm meter as speed output AO Attachmentdetails og motor and drive.zip (476 Downloads) |
6/10/2022 6:53 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please refer SINAMICS G120 Power Module getting started & SINAMICS G120 PM240 Power Modules hardware installation manuals, may help you. |
Last edited by: Jen_Moderator at: 06/10/2022 11:36:01Links optimized. |
|
This contribution was helpful to
1 thankful Users |
6/11/2022 11:53 AM | |
Joined: 4/6/2021 Last visit: 2/13/2025 Posts: 22 Rating:
|
Sir Need to comission this drive.pleasr guide |
6/14/2022 10:29 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Please refer attached project wherein you will find predefined parameter values of your project. BTW which is CU? In project P presumed CU240E. If want more details, please provide electrical wiring diagram along with CU & application details. HTH AttachmentTRIAL DEL.zip (501 Downloads) |
6/15/2022 10:44 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 4/6/2021 Last visit: 2/13/2025 Posts: 22 Rating:
|
Sir Thanks for support. Please find attached file for Motor name plate details and connection drawing. Old 45Kw motor was running OK. did the quick commissioning for Required 75KW motor and put the parameter as below. during trial, Drive was tripping on motor data mismatch fault.so did the sand still ID run By P1900=2 after that not motor tripping found. Motor run from BOP .Motor is Rotating, but after 67 RPM Speed Motor getting heavy jerk and speed is reducing to 37 -40RPM.seen motor taking full current , voltage is 576V and Frequency was 1.1 Hz. further increasing the speed from BOP, refence feedback is increasing , but motor is rotating with 37 -40 rpm and actual speed. not increasing the speed. Motor Resistance and megger value is OK. Shaft is not Jam Please suggest
AttachmentG 120.docx (498 Downloads) |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
6/15/2022 10:53 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Which is Control Unit? CU 230 or CU240 or CU250 etc. etc.? |
6/15/2022 12:18 PM | |
Joined: 4/6/2021 Last visit: 2/13/2025 Posts: 22 Rating:
|
Control unit is CU250S-2 USS |
Follow us on