12/2/2018 5:31 PM | |
Posts: 2826 Rating:
|
Hello.
@dchartier: Said with respect - the link you have given is not directly helpful. The question is from the viewpoint of the HMI; not the the viewpoint of the PLC. @EduardoFS: A quick search did not produce the answer I hoped to present you. It depends on the class of HMI / SCADA what the maximum connections it can have. When using Siemens products we use the KTP700PN. The following image shows that defining 5 connections gives a problem, while 4 is okay. Another article to look at is: There other ways of doing this task, also including non-siemens products. Best to do some web research on that. Another approach is to have a PLC that links as a server between the machines to the HMI. For this case, Mr. Chartier's provided link is helpful. Yet another idea is to use an IOT2000 as data server (read: middleman). It is best to create topics at the relevant conferences stating detailed questions if you think these ideas are worth following up on. Regards. |
This contribution was helpful to
1 thankful Users |
12/3/2018 3:24 PM | |
Posts: 2826 Rating:
|
See attached an archive file that consists of three short movies. Tags are linked from multiple PLCs to one HMI. The created tags can then be used in the development of the HMI just as one would for one HMI and one PLC. Are the movies helpful? Attachmentmulti-plc-to-hmi.zip (226 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on