10/1/2021 9:07 AM | |
Joined: 4/28/2015 Last visit: 12/8/2023 Posts: 3298 Rating:
|
Hi, the Industrial OS is not pre-configured with IP addresses, as the Example Image is. When you boot the Industrial OS for the first time you should end up in a configuration, where you can setup users/password, network interfaces, etc. Unfortunately this needs to be done in order to change the boot order from the Industrial OS. An alternative is using an UART cable to establish a serial connection. With that you can change the boot order before booting into the OS. Please check the document in this post for more details:
Best regards! |
This contribution was helpful to
1 thankful Users |
10/1/2021 5:05 PM | |
Posts: 2 Rating:
|
Thank you. Everything worked fine with your instructions. |
This contribution was helpful to
1 thankful Users |
Follow us on